Search FAQs
Video: How do you set up the ATV630 process drive so HMI dial is speed reference and the terminals are start stop control?
Issue:
ATV630 set up to work HMI as speed reference and terminals as start stop control.
Product Line:
Altivar ATV630 and ATV930 drives
Environment:
All
Cause:
HMI speed reference and terminal 2 wire control for starting.
Resolution:
Programming Sequence
From the Main Menu:
ATV630 set up to work HMI as speed reference and terminals as start stop control.
Product Line:
Altivar ATV630 and ATV930 drives
Environment:
All
Cause:
HMI speed reference and terminal 2 wire control for starting.
Resolution:
Programming Sequence
From the Main Menu:
- Scroll down (slide your finger around the wheel clockwise) to Menu 5 Complete Settings and press OK
- Then scroll down to Menu 5.5 Command and references, press OK, and verify/modify the following parameters:
- Ref Freq 1 Config = Ref.Freq-Rmt.Term (sets the keypad to be your speed control)
- control mode = Separate (your start/stop command and speed reference are coming from different sources)
- Command switching = Command channel 1 (tells the drive to look at channel 1 for start/stop)
- CMD channel 1 = Terminals (tells the drive what command channel 1 is)
However, going from I/O Profile to Not Separate would force a factory reset. So if you're already set to I/O Profile, leave it in I/O Profile unless you want to do a factory reset.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: