{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert - Why doesn't auto-diagram work for my custom device created in the Modbus Device Importer?
Issue
'Add "Generate Network Diagram" Support' in the Modbus Device Importer does not write to the DeviceInfo registry key, and thus Vista 'auto-diagram' will not work.

Product Line
Power Monitoring Expert (PME) 7.2.x, 8.x, 9.0
StruxureWare Power Monitoring 7.0.x
ION Enterprise

Environment
Modbus Device importer (MDI)

Cause
User running the MDI program does not have permission to write to the registry

Resolution

To correct this problem, either populate the Registry manually (not recommended) or launch MDI as user with permissions to write to the registry and re-run the 'Add "Generate Network Diagram" Support' menu item.

1) Locate the ModbusDeviceImporter in [PME install folder]\system\bin
2) Right click and select "Run as administrator"

Note: In PME 9, Device Type Editor (DTE) is used to add diagram support. The DTE may also need to be run as Administrator

Schneider Electric Egypt and North East Africa