Search FAQs
Video: How do I disable the Output Phase Loss on an Altivar ATV630 Process Drive?
Issue:
Disabling OPL on an ATV630 process drive.
Product Line:
ATV630 process drive
Environment:
All models and serial numbers
Appl. V1.3 IE 07
MC: V1.3 IE 07
Cause:
None
Resolution:
Go to menu 5 => [Complete settings] => 5.12 [Error/Warning handling] => [Output Phase Loss]
Setting Code / Value Description
[Function Inactive] nO Function inactive
[OPF Error Triggered] YES Tripping on [OutPhaseLoss Assign] OPL with freewheel stop - Factory setting
[No Error Triggered] OAC No detected error triggered, but management of the output voltage in order to avoid an overcurrent when the link with the motor is reestablished and catch on the fly performed (even if this function has not been configured).The drive switches to [Output cut ]SOC state after [OutPhL Time] Odt time. Catch on fly is possible as soon as the drive is in stand by output cut [Output cut] SOC state.
Disabling OPL on an ATV630 process drive.
Product Line:
ATV630 process drive
Environment:
All models and serial numbers
Appl. V1.3 IE 07
MC: V1.3 IE 07
Cause:
None
Resolution:
Go to menu 5 => [Complete settings] => 5.12 [Error/Warning handling] => [Output Phase Loss]
Setting Code / Value Description
[Function Inactive] nO Function inactive
[OPF Error Triggered] YES Tripping on [OutPhaseLoss Assign] OPL with freewheel stop - Factory setting
[No Error Triggered] OAC No detected error triggered, but management of the output voltage in order to avoid an overcurrent when the link with the motor is reestablished and catch on the fly performed (even if this function has not been configured).The drive switches to [Output cut ]SOC state after [OutPhL Time] Odt time. Catch on fly is possible as soon as the drive is in stand by output cut [Output cut] SOC state.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: