{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

CAN NSX AC BREAKER be USED IN DC APPLICATIONS ?

  • ONLY the following 2 categories of the compact NSX AC MCCB are proven to operate under DC rated operatinal voltage as shown in the attached catalogue Panorama.
1- The compact NSX AC MCCB 1 Pole - from 100 to 250A only -  can be used under 250VDC rated operational voltage .
2- The compact NSX AC MCCB 2 Poles - from 100 to 250A only - can be used under 500VDC rated operational voltage.
  • Kindly use the below link to download the Schneider offer for DC networks Circuit breakers from 16 to 4000A Compact NSX DC & Masterpact NW DC.
  • https://www.se.com/uk/en/download/document/LVPED208006EN/

Schneider Electric Egypt and North East Africa