{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you take the ATV212 drive out of PID mode and control the drive locally by pushing the local remote button?
Issue:
Wanting to take the ATV212 drive out of PID mode and control the drive locally by pushing the local remote button.

Product Line:
Altivar 212, S-FLEX 212, Altivar Machines

Environment:
All

Cause:
N/A

Resolution:
When the Altivar 212 drive is in PID control, pressing LOC/REM to go to Local mode does NOT deactivate PID control.  Local mode will provide HMI RUN / STOP control and HMI adjustment to the PID setpoint.  The drive will stay in PID control regardless of the Local/Remote setting on the drive. 
To deactivate  PID control, assign a logic input to function 14 (PID disable).  When the specified assigned input is energized, the drive will be taken out of PID mode.  Control will then be based on normal CMOd and FMOd assignments.  The VFD can also then be put into Local mode, via the LOC/REM button, for HMI control of RUN / STOP and HMI speed adjustment.

To go back to PID control, de-energize the specified assigned input.
NOTE:  If the VFD is setup for PID setpoint via the HMI, then the Local mode adjustment of speed via the HMI will also adjust the PID setpoint.

Programming Example
F360 set to 1
FMOD set to 3
Drive is in PID mode on VIA for 4-20mA signal. The HMI can be used to adjust the set point. (Toggling between LOCAL/REMOTE will keep the drive in PID mode regardless)

Set F112 = 14 (set LI R selection to PID deactivate)
When terminal logic input R is energized then the drive is taken out of PID mode.

Schneider Electric Egypt and North East Africa

Attachment(s)
S1A53838 ATV212 programming manual.pdf [3.52 MB]
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.