Search FAQs
Can a port number other than Modbus/TCP port 502 be used for I/O Scanning on the 140CPU6xxxx native ethernet port?
Product Line:
Quantum PLC
Environment:
EcoStruxure Control Expert
Resolution:
No, the Quantum 140CPU6xxxx Copro native ethernet port will only use Modbus TCP port 502 when performing an I/O Scanning function.
Port 502 is hard-coded into the Ethenet port settings and is not configurable.
Quantum PLC
Environment:
EcoStruxure Control Expert
Resolution:
No, the Quantum 140CPU6xxxx Copro native ethernet port will only use Modbus TCP port 502 when performing an I/O Scanning function.
Port 502 is hard-coded into the Ethenet port settings and is not configurable.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: