Search FAQs
How come the GVL (Global Variable List) variables are not showing up in Symbol Configuration of SoMachine / EcoStruxure Machine Expert?
Issue:
How come the Global Variable List (GVL) variables are not showing up in Symbol Configuration of SoMachine / EcoStruxure Machine Expert?
Product Line:
GVL, Global Variable List, Symbol Configuration, SoMachine v3.x, SoMachine v4.x, EcoStruxure Machine Expert v1.x / v2.0
Resolution:
In order for the GVL Variables to show up in the Symbol Configuration window, at least one of the variables in the GVL node must be used in logic.
These criteria must be met:
1) The GVL variable is referenced or used in a Program Organization Unit (POU).
2) The POU that the GVL is used in has been added to an Application Task (for example under "Task Configuration -> MAST")
How come the Global Variable List (GVL) variables are not showing up in Symbol Configuration of SoMachine / EcoStruxure Machine Expert?
Product Line:
GVL, Global Variable List, Symbol Configuration, SoMachine v3.x, SoMachine v4.x, EcoStruxure Machine Expert v1.x / v2.0
Resolution:
In order for the GVL Variables to show up in the Symbol Configuration window, at least one of the variables in the GVL node must be used in logic.
These criteria must be met:
1) The GVL variable is referenced or used in a Program Organization Unit (POU).
2) The POU that the GVL is used in has been added to an Application Task (for example under "Task Configuration -> MAST")
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: