{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
If an application built for a lower level M580 HSBY CPU can be downloaded & executed in a higher level M580 HSBY CPU?

Article available in these languages: Spanish

Yes,an application built for the BMEH582040 is downloadable and executable on the BMEH584040, BMEH586040.
An application built for the BMEH584040 is downloadable and executable on the BMEH586040.

Schneider Electric Egypt and North East Africa