What is the actual current consumption of a Lexium Integrated Drive type ILA ?
The current consumption printed on the motor label is value used for UL rating and does not reflect actual current consumption under normal operating conditions.
The real current consumption depends on: - motor speed - torque - power supply voltage - acceleration with load inertia - The number of motors which are running at the same time - current reduction at standstill activated
The real nominal current can be estimated as follow:
Pmechanic = 2*pi * n * M
(n : rps, M : Nm)
Current consumption = (Pmechanic + electrical losses) / Power Supply Voltage
(electrical losses for ILA2T round about 30 W)
Two example:
1. Power Supply Voltage = 24VDC: n = 100rpm = 1,666rps, M = 3Nm
Pmechanic = 2* pi * 1,666rps * 3Nm Pmechanic = 31,4 W
Current consumption = (31,4 W + 30 W) / 24VDC Current consumption ~ 2,5A
2. Power Supply Voltage = 48VDC: n = 100rpm = 1,666rps, M = 3Nm
Pmechanic = 2* pi * 1,666rps * 3Nm Pmechanic = 31,4 W
Current consumption = (31,4 W + 30 W) / 48VDC Current consumption ~ 1,3A
Rev 2-20-18
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Lexium ILA, ILE, ILS
Lexium ILT, ILP
Lexium 32i
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.