{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the signal range for Netbotz wireless sensors?
Issue:
How far can NetBotz wireless devices communicate?

Product Line:
Netbotz Appliance

Environment:
Netbotz Appliance Version

Cause:
Expected range of NetBotz wireless sensors.

Resolution:

Supported devices on the NetBotz wireless network

The Wireless Temperature Sensor is always configured as an End Device in your wireless sensor network.

The following wireless devices can be configured as a Coordinator or Router:

Sensor Name                                          Range                Part Number
NetBotz USB Coordinator & Router     100 ft-line of sight     NBWC100U
NetBotz Wireless Sensor Pod 180      100 ft-line of sight     NBPD0180

The following wireless devices can be configured as an End Device:

Sensor Name                                          Range                Part Number
NetBotz Temperature Sensor            100 ft -line of sight     NBWS100T/ NBWS100H
NetBotz Wireless Sensor Pod 180         100 ft -line of sight     NBPD0180

Schneider Electric Egypt and North East Africa