{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PM8000 Is Unable To Send Emails
Issue
The PM8000 will not send an email even when the Alert module is setup correctly and on the same network as the SMTP server.

Product Line
PM8000

Environment
Sending alert via SMTP

Cause
This is an issue with all PM8000 firmware versions including and prior to V001.003.001 interacting with some SMTP servers. The PM8000 is able to connect SMTP server; however, the request is rejected with the error, "HELO requires domain address." This can be seen in a Wireshark capture:
No.TimeSourceDestinationProtocolLengthInfo
<PM8000><SMTP server>SMTP60HELO
<SMTP server><PM8000>SMTP94HELO requires domain address

Resolution
This is a known issue and has been corrected in the firmware version V001.004.001
Notes
For instructions on upgrading the firmware using ION Setup please follow our knowledgebase article FA244316

Schneider Electric Egypt and North East Africa