{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the High Altitude De-rating (Re-rating) requirements for an I-Line panelboard?
Issue:
High Altitude De-rating requirements for I-Line panelboard

Product Line:
i-Line Panelboard

Environment:
Products sold and used in North America

Cause:
Installation / Setup

Resolution:
Only the circuit breakers in an I-Line panelboard require de-rating (re-rating) for high altitude applications. The bus assembly in the Panelboard is not affected by high altitude and can be used at it's full rating. Tables showing how to de-rate (re-rate) the circuit breakers can be found in Data Bulletin 0100DB0101 which is attached below.

Schneider Electric Egypt and North East Africa

Attachment(s)
0100DB0101 Determining Current Carrying Capacity in Special Applications.pdf [86.96 KB]