{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the smallest size motor that can used on the ATS22 Soft Starters?
Issue:
Smallest size motor that can used on the ATS22 soft starters

Product Line:
Altistart ATS22

Environment:
All

Cause:
N/A

Resolution:
The rated motor current can be programmed to 40% of the Soft starters current ratings.
Example if the Soft starter rated current (IcL) is 17 amps you can decrease the motor nominal current (In) parameter of the soft starter to as low as 40% or 17*.4 = 6.8 amps.

Schneider Electric Egypt and North East Africa

Attachment(s)
ats22_user_manual_en_bbv51330_02.pdf [3.02 MB]