{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a 63.75" tall PDU be installed into a 38U NetShelter CX cabinet?
Issue:
The 63.75" tall PDU does not fit onto the accessory rail. Will it fit anywhere else inside the cabinet?

Product Line:
NetShelter CX

Environment:
AR4038A, AR4038IA

Cause:
One of the 63.75" tall PDUs has been specc'd into a 38U NetShelter CX cabinet.

Resolution:
Yes, the 63.75" tall PDUs can attach to the rear mounting rail. Please see the attached file for mounting instructions.

Schneider Electric Egypt and North East Africa

Attachment(s)
20160729 Tall PDU Mounting Into 38U NetShelter CX.docx [5.95 MB]