Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What are the reasons for system fault code 49 on LTMR08MFM (Motor Management SYSTEM )

Fault Code 49 = Stop Checkback

The LTM R controller performs diagnostic tests that detect and monitor the proper functionality of control

commands.

There are 4 control command diagnostic functions:

 Start Command Check

 Run Check Back

 Stop Command Check

 Stop Check Back

 

Stop Check Back

The Stop Check Back causes the LTM R controller to continuously monitor the main circuit to ensure no

current is flowing. The Stop Check Back:

 reports a Stop Check Back fault or warning if average phase current is detected for longer than 0.5

seconds without a Run command, or

 ends, when a Run command executes

Actions that can be taken :
 

Check the following:

 relay outputs

 all wiring, including:

 control wiring circuit, including all electromechanical devices

 power wiring circuit, including all components

 load CT wiring.

After all checks are complete:

1 Reset the fault.

2 If the fault persists, cycle power and wait 30 s.

3 If the fault persists, replace the LTM R controller.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: