{}

Our Brands

Impact-Company-Logo-English Black-01-177x54
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
How can we help you today?
What is the difference between the Altivar 630 drive and the Altivar 930 drive?

Article available in these languages: Spanish, Turkish

Issue:
Difference between the Altivar 630 and the Altivar 930 drives?

Product Line:
Altivar 630 and Altivar 930 Series

Environment:
All serial numbers for Altivar 630 and Altivar 930 Series

Cause:
N/A

Resolution:

-The Altivar 630 is designed for Variable torque application similar to the Altivar 61 drives and includes a lot of additional pump control and monitoring functions.
-The Altivar 930 is designed for the Constant torque applications and built for the heavy machinery applications similar to the Altivar 71 drives.
-Click on each link above to access the installation manual for the ATV630 Drive and the ATV930 Drive to see more detailed features between the two drives.   Also note that the ATV630 has built in Ethernet TCP-IP and the ATV930 Drive has built in Ethernet TCP-IP and Ethernet IP.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.