Issue
Want to know what values are linked to the SNMP Mapping module in the PM8000.
Product Line
PowerLogic PM8000 series meter
Environment
Advanced metering offer
Resolution
Simple Network Management Protocol (SNMP) is part of the Transmission Control Protocol/Internet Protocol (TCP/IP) protocol suite. It is an application layer protocol that facilitates the exchange of network management information between devices, allowing you to manage network performance and to identify and solve problems on networks with devices of various types.
PM8000 meter supports SNMP once SNMP is activated on the meter. The meter's MIB file needs to be upload into the NMS managing your meter. See FA276689 for more details about setting SNMP. The MIB file is included with the meter's Firmware ZIP file located on se.com.
*Warning: Changing your meter’s default SNMP configuration assumes that you have an advanced understanding of ION architecture, SNMP, and the communications network and power system that your meter is connected to.
Enabling SNMP provides SNMP access to the meter values linked to the SNMP Mapping module. You can configure the SNMP Mapping module to link to different meter values. By default, the following meter values are linked to the SNMP Mapping module:
The following meter information is always provided by default and cannot be configured:
Voltsmode, Model number, Serial number, Device name, Firmware version, MIB version
Note: If you change your meter’s default values you must modify the default MIB file to reflect the new values.
Want to know what values are linked to the SNMP Mapping module in the PM8000.
Product Line
PowerLogic PM8000 series meter
Environment
Advanced metering offer
Resolution
Simple Network Management Protocol (SNMP) is part of the Transmission Control Protocol/Internet Protocol (TCP/IP) protocol suite. It is an application layer protocol that facilitates the exchange of network management information between devices, allowing you to manage network performance and to identify and solve problems on networks with devices of various types.
PM8000 meter supports SNMP once SNMP is activated on the meter. The meter's MIB file needs to be upload into the NMS managing your meter. See FA276689 for more details about setting SNMP. The MIB file is included with the meter's Firmware ZIP file located on se.com.
*Warning: Changing your meter’s default SNMP configuration assumes that you have an advanced understanding of ION architecture, SNMP, and the communications network and power system that your meter is connected to.
Enabling SNMP provides SNMP access to the meter values linked to the SNMP Mapping module. You can configure the SNMP Mapping module to link to different meter values. By default, the following meter values are linked to the SNMP Mapping module:
I a | kVAR tot | Vll ca | Vln avg | Ib mean | kW sd mx del-rec |
I b | kVA tot | Vll avg | Freq | Ic mx | kW sd del |
I c | PF sign tot | Vln a | Ia mx | Ic mean | kW sd rec |
I avg | Vll ab | Vln b | Ia mean | kW sd mx del | kW sd del-rec |
kW tot | Vll bc | Vln c | Ib mx | kW sd mx rec | kVAR sd mx del |
kVAR sd mx rec | kVAR sd mx del-rec | kVAR sd del | kVAR sd rec | kVAR sd del-rec | kVA sd mx del |
kVA sd mx rec | kVA sd mx del-rec | kVA sd del | kVA sd rec | kVA sd del-rec | kWh del |
kWh rec | kWh del-rec | kVARh del | kVARh rec | kVARh del-rec | kVAh del |
kVAh rec | kVAh del-rec |
The following meter information is always provided by default and cannot be configured:
Voltsmode, Model number, Serial number, Device name, Firmware version, MIB version
Note: If you change your meter’s default values you must modify the default MIB file to reflect the new values.