{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert 8.1 - Web Application is not beeping for Unacknowledged Alarms
Issue
After upgrading from PME 8.0 to PME 8.1, the Web Application no longer gives an audible alert for Unacknowledged alarms that are no longer active.

Product Line
Power Monitoring Expert 8.1

Environment
Web Applications

Cause
The audible alarm alert performance was changed between PME 8.0 and PME 8.1. See the tables below:

PME 8.0
Active AlarmsHistorical Alarms
Unacknowledged AlarmsAudible AlertAudible Alert
Acknowledged Alarms

​PME 8.1
Active AlarmsHistorical Alarms
Unacknowledged AlarmsAudible Alert
Acknowledged Alarms

In Power Monitoring Expert 8.0, an Audible Alert will sound for all Unacknowledged Alarms, regardless if the alarm is active or inactive.
In Power Monitoring Expert 8.1, an Audible Alarm will only sound for Unacknowledged Active Alarms.

Resolution:
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*


1) Open the attached .sql file in SQL Server Management Studio
2) Configure the 'SET Value =' to the desired behavior.
'true' = This will activate Audible alerts when there are Unacknowledged alarms.
'false' = This will activate Audible alerts only when there are Active alarms (default setting).
The Application Modules services do not need to be restarted after the query is executed as the change is picked up automatically.

Note: This article applies only to Power Monitoring Expert 8.2. In Power Monitoring Expert 9.0, the behavior of the audible alerts is now configurable in the Web Applications under Settings > Alarm Views

Schneider Electric Egypt and North East Africa