{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is PME a multithreaded application?
Issue
Is PME a multithreaded application? If so, does its multiple threads run on different processors? Or, is it a single-threaded application?

Product Line
PME 8.x, 7.2.x

Environment
PME supported Windows OS.

Cause
Customer is curious to know whether PME runs on one thread or multiple threads? Is it capable of making use of multiple processors at the same time?

Resolution
PME consists of many applications. By design, they are all multi-threaded and will run across multiple processors.

Schneider Electric Egypt and North East Africa