{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Unity Momentum use Base 0 or Base 1 addressing? (Unity is now referred to as Control Expert)
The Unity Momentum processors use a Base 1 address. The first reference(s) will be %MW1, %IW1, %M1,%I1.
By using the same Base address as the legacy Momentums the process of  migrating to Unity is further simplified.
(Unity Pro is now referred to as Control Expert)

Schneider Electric Egypt and North East Africa