{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will the ATV320 be available above 5HP in 480V compact version?
Issue:
ATV320 availability above on 5HP in 480V compact version.

Product Line:
ATV320 series

Environment:
Compact version (C)

Cause:
Information unavailable or difficult to find in current literature.

Resolution:
The ATV320 series, 480V rating, will only be available up to 5HP in the compact (C) version.  Above 5HP, the Book (B) version will be available from 7.5HP to 20HP.

Schneider Electric Egypt and North East Africa