Issue:
Part number for the RFI filter grounding jumper for the ATV61HC11N4 Drives?
Product Line:
Altivar ATV61
Environment:
Only Frame size 9 ATV61 or ATV71 drives
Cause:
Customer removed and lost the RFI filter ground jumper and need to get a replacement.
Resolution:
The RFI jumper is included as part of a Field Services only order kit part VY1A1303.
This part only can be ordered thru field services only.
I have attached a sheet of all of the parts that are included in the VY1A1303 kit. The jumper part is not sold by its self.
This kit applies to Size 9 ATV61 and ATV71 drives only which are the ATV61HC11N4, ATV61HD90N4 and ATV71HD90N4
Part number for the RFI filter grounding jumper for the ATV61HC11N4 Drives?
Product Line:
Altivar ATV61
Environment:
Only Frame size 9 ATV61 or ATV71 drives
Cause:
Customer removed and lost the RFI filter ground jumper and need to get a replacement.
Resolution:
The RFI jumper is included as part of a Field Services only order kit part VY1A1303.
This part only can be ordered thru field services only.
I have attached a sheet of all of the parts that are included in the VY1A1303 kit. The jumper part is not sold by its self.
This kit applies to Size 9 ATV61 and ATV71 drives only which are the ATV61HC11N4, ATV61HD90N4 and ATV71HD90N4
Released for:Schneider Electric Egypt and North East Africa