Product Line
ION Setup 3.0
ION Setup 3.1
ION Setup 3.2
Environment
Software Installation
Resolution
ION Setup 3.0 (Build 3.0.16218.01) and later versions are supported on Windows 10.
The latest version can be downloaded using the link below:
ION Setup Software
Note: ION Setup is still not UAC compliant. When installing ION Setup, log in with an Administrator account and right-click the installer to select "Run as Administrator".
ION Setup 3.0
ION Setup 3.1
ION Setup 3.2
Environment
Software Installation
Resolution
ION Setup 3.0 (Build 3.0.16218.01) and later versions are supported on Windows 10.
The latest version can be downloaded using the link below:
ION Setup Software
Note: ION Setup is still not UAC compliant. When installing ION Setup, log in with an Administrator account and right-click the installer to select "Run as Administrator".
Released for:Schneider Electric Egypt and North East Africa