Search FAQs
Is the DC Choke included in a High HP ATV61 or ATV71 drive?
Issue:
Customer wants to know if the DC Choke comes with the drive or if it needs to be ordered separately.
Product Line:
ATV61:
ATV71:
Part numbers MUST NOT have a D at the end.
Environment:
All versions
Cause:
Clarification of part numbers
Resolution:
The ATV61 and ATV71 High HP drives come standard with the DC Choke.
However, part numbers with a D at the end (example; ATV61HC11N4D) have the DC Choke deleted and will REQUIRE the use of a 5% input line reactor.
See the installation manual (https://www.se.com/us/en/download/document/1760655/) for details if needed.
Customer wants to know if the DC Choke comes with the drive or if it needs to be ordered separately.
Product Line:
ATV61:
55 kW (75HP) thru 90 kW (125 HP) at 200-240 VAC
90 kW (125HP) thru 630 kW (900 HP) at 380-480 VAC
90 kW (125HP) thru 630 kW (900 HP) at 380-480 VAC
ATV71:
55kW (75HP) thru 90 kW (100 HP) at 200-240 VAC
90 kW (125HP) thru 630 kW (700 HP) at 380-480 VAC
90 kW (125HP) thru 630 kW (700 HP) at 380-480 VAC
Part numbers MUST NOT have a D at the end.
Environment:
All versions
Cause:
Clarification of part numbers
Resolution:
The ATV61 and ATV71 High HP drives come standard with the DC Choke.
However, part numbers with a D at the end (example; ATV61HC11N4D) have the DC Choke deleted and will REQUIRE the use of a 5% input line reactor.
See the installation manual (https://www.se.com/us/en/download/document/1760655/) for details if needed.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: