{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What could have cause the Magelis target to get a timeout error when communicating to the Somachine controller using the Somachine protocol?
Issue:
What could have cause the Magelis target to get a timeout error when communicating to the Somachine controller using the Somachine protocol?

Product Line:
M238, M241, M251, M258, HMISTO/STU, HMIGTO/GTU, XBTGH/GK/GT, Panel PC, Box PC

Resolution:
Most communications issues between the Magelis and Somachine controller has to do with the Nodename of the controller does not match.  Go to the Vijeo Designer, for MyController under the Somachine protocol of the IO Manager.  The node name in that field must match the controller Node name.  Once that has been modified, download to the Magelis and see if the communications will establish.

Schneider Electric Egypt and North East Africa