{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: Data Center Expert | How do I enable surveillance for NetBotz cameras?

Issue:
Enabling surveillance in StruxureWare Data Center Expert for NetBotz cameras.

Product Line
StruxureWare Data Center Expert (DCE)
- Basic Appliance (AP9465)
- Standard Appliance (AP9470)
- Enterprise Appliance (AP9475)
- Virtual Appliance (AP94VMACT)
StruxureWare Central (SWC)
InfraStruXure Central (ISXC)
NetBotz v3 Wall Appliance: 355/356 (NBWL0355/6) & 455/456 (NBWL0455/6)
NetBotz v3 Rack Appliance: 450/451 (NBRK0450/1), 550 (NBRK0550), & 570 (NBRK0570)
NetBotz Rack Monitor 750 (NBRK0750)

Environment:
StruxureWare DCE (any version)
NetBotz discovered by DCE (any supported version)

Cause:
This is for customers that require assistance in enabling surveillance for NetBotz cameras in DCE

Resolution:

  1. Log into the Data Center Expert client.
  2. Ensure that the NetBotz Appliance with an integrated or attached camera pod is showing within Data Center Expert.  If it has not been discovered yet, reference FA177081.
  3. Each NetBotz camera requires one Surveillance license.  You can verify the licensing that you have installed by going to: System Menu > Server Administration Settings > License Keys.  There will be a specific license type of Surveillance Pack with a total column and a used column.
  4. Select the Surveillance perspective.
  5. Right-click on one of the camera thumbnails and select Surveillance settings. TIP: You can select multiple thumbnails by holding down CTRL or SHIFT and selecting them.
  6. Mark the check box for License Camera.
  7. Enter the Data Center Expert IP address and configure the security options if necessary.
  8. Select the Post Mode that you would like to record the Surveillance clips for.  There are other options to configure if deemed necessary.
  9. Select Apply and OK.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Data Center ExpertNetBotz 400NetBotz 300NetBotz 500
Explore more
Range:
Data Center ExpertNetBotz 400NetBotz 300NetBotz 500
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.