{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a BCPME042S use 84 CTs?
Product Line
BCPME (Branch Circuit Power Monitor)

Environment
Operation

Cause
The BCPME 42 (2 CT Strips) and 84 (4 CT Strips) models look the same. They share the CT Panel layout with both Panel 1 and Panel 2
BCPME 42

Resolution
The 42 CT model cannot use 84 CTs even though it can connect the extra two strips to accommodate it. The 42 CT model does not have Panel 2 wired, which prevents them from being capable of being used. These connectors are left on the meter in order to reduce cost in manufacturing.

Schneider Electric Egypt and North East Africa