Search FAQs
Is there an address to read status of the RJ-45 ports on the Altivar Process Profinet Card?
Issue:
Address to read status of the RJ-45 ports on the Process Profinet Card.
Product Line:
ATV630, Altivar 630, Altivar Process
Environment:
All
Cause:
Customer wants to know if Port A or Port B on the Profinet Card is up or down
Resolution:
With last version of Profinet V1.6, it's not possible to see the port status with Modbus address or PNU address. The information is not accessible this way. However, you can read status only by LLDP service. See attachment.
Address to read status of the RJ-45 ports on the Process Profinet Card.
Product Line:
ATV630, Altivar 630, Altivar Process
Environment:
All
Cause:
Customer wants to know if Port A or Port B on the Profinet Card is up or down
Resolution:
With last version of Profinet V1.6, it's not possible to see the port status with Modbus address or PNU address. The information is not accessible this way. However, you can read status only by LLDP service. See attachment.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: