{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
[UP11] Why more than one M580 IOscanning rows are removed even i only removed one row.
Question:
After removing row number5 of Ioscaning from M580 Ioscanning list;

you will see only last two rows leave, all others are removed..


Answer:
Actually, it is not an issue, more than one Ioscanning rows be removed after you remove one row is because the  scroll bar of Ioscanning window is automatically moved to the bottom, so you can only see the last two rows of Ioscanning.
move the scroll bar back to the top then you can see all the rest Ioscanning rows.

Schneider Electric Egypt and North East Africa