{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Unity Pro, what is occurring on Save/Restore Data containing forced bit?
Saving data containing forced bit by the command «PLC/Save Data From PLC to file» save also the Forced state of these bit .
When these bit will be restored by the command «PLC/Restore Data From to file to PLC»  they will be restored in Forced state.
Nevertheless the list of forced bit will not be restored and in final bit will be forced in the application without knowing easily which ones.
So it is strongly recommended to do not save data with forced bit in the application.

This behavior is always present in Unity Pro V11.1  it is planned to be fixed in a next version.
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.