{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is SoMachine V4.1 SP2 compatible with Windows 10?
Issue:
SoMachine V4.1 SP2 windows compatibility

Product Line:
SoMachine

Resolution:
SoMachine V4.1 SP2 supports Windows 7, 32 and 64 bit, as well as Windows 8.1, 32 and 64 bits only.
SoMachine V4.2 supports Windows10.

Schneider Electric Egypt and North East Africa