{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to archive a Unity applications with remote BMXPRA0100 programs.
Title
Archive a Unity applications with remote BMXPRA0100 programs

Issue
Archive a Unity applications with remote BMXPRA0100 programs

Product Line
M340 BMXPRA0100

Environment
Unity Pro

Cause
N/A

Resolution
After your BMXPRA0100 Unity application is configured: (Built and downloaded to the BMXPRA0100)
You need to use the Export or Save Archive function for your BMXPRA0100 application before you Close the BMXPRA0100 application instance of Unity Pro
NOTE: When You are asked if you want to save the PRA application in the master application *.stu file, answer YES.
Then the PRA application is saved (embedded) in the master application. If you select No, all changes are lost.
When sending the application to another person, create a .ZEF copy of the Master M340 application.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: