{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you set up preset speeds on the Altivar 630 Process drive using the Somove Software?
Issue:
Can I use SoMove to set up preset speeds on the ATV630 drive?

Product Line:
Altivar ATV630 and ATV930 drives

Environment:
All

Cause:
Wants to setup preset speeds using somove software

Resolution:
Open Somove file
Goto Parameter Layout
Preset Speeds
PS2 set to LI3
SP2 set to 60hz.

Schneider Electric Egypt and North East Africa