{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

Video: How to change the Coil Fluid Temperature Thresholds on a Network Air FM Unit

Issue:
This document contains a video of how to change the Coil Fluid Temperature Thresholds on a Network Air FM Unit.

Product line:
FM 35-50, IR40, ACFM400, ACFM200.

Environment:
All Serial Numbers.

Cause:
Install, Configuration.

Resolution:



To change or set the coil fluid temperature threshold.

Press the ESC Key until you get to the main menu.

Press ENTER on Setup.

Press ENTER on System 1.

Press ENTER on Alarms.

Scroll down to Coil Fluid Thrshlds and press ENTER.

Using the UP or DOWN arrows you can select the High or Low threshold.

Press ENTER on either then change the value with the UP or DOWN arrow.

Finish by pressing the ENTER key and then press ESC until you get to the status menu.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: