Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How Can I establish communication between Micom P141 or P143 to ABB RTU through IEC61850 protocol since when Im trying to add MCL file it became freezed
You need to use Easergy studio V7.0.0 then after creating a system file, add a new device P141 you can follow the procedure attached
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: