{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

NetBotz 250A | How do I update the firmware?

Issue:
Process for updating firmware on the NetBotz Rack Monitor 250(A).

Product Line:
NetBotz Rack Monitor 250 (NB250)

Environment:
NetBotz Rack Monitor 250 (all firmware versions)

Cause:
You must update the firmware on the Rack Monitor 250(A) to the most recent version before first use.

Resolution:

NOTE: The NetBotz 250 appliances must be communicating on the network to be able to upgrade the firmware using this option.  Steps for setting the IP address can be found within knowledge base NetBotz 250 | Configuring Network Settings .

1) Download the most recent firmware in the Download sections of the NetBotz 250 product page on APC.com.

2) Run the executable that downloads, which will extract the necessary upgrade files and automatically run the Upgrade Wizard Utility.

3) If only upgrading one appliance, enter the IP Address, username, and password.  If upgrading multiple appliances, check the box for Upgrade from Device List, and fill in the Device List option.

4) Select Ping to test network connectivity to the appliances.

5) Select Upgrade Now to issue the upgrades to the appliance(s).

NOTE: Other firmware upgrade procedures are available within knowledge base Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)? .

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: