Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What are the Sepam 40 & 80 firmware requirements for setting up the ACE850TP / ACE850FO
Issue
Want to be able to communicate over TCP/IP and was wondering if the old Sepam in the field has the ability.
 
Product Line
ACE850TP/ ACE850FO
 
Resolution
The Sepam 40 and Sepam 80 must have a minimum firmware shown in the below table.  
 
ACE850 (TP/FO)Version OK
Sepam Series 40V7.00 or Greater
Sepam Series 80Base & Application V6.00 or Greater

Note: That the ACE850 cannot be used with the Sepam 20 series.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: