{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What are the G1, G2, G3 and Gx classifications for the ANSI Standard, ANSI/ISA S71.04-1985, “Environmental Conditions for Process Measurement and Control Systems: Airborne Contaminants,”?
The G3 specification references the ANSI Standard, ANSI/ISA S71.04-1985, “Environmental Conditions for Process Measurement and Control Systems: Airborne Contaminants,” .

The G reference refers to the severity and classification of the test and it can be G1 (Mild, Moderate, Harsh and Severe (G1, G2, G3 and Gx, respectively).  The classification directly correlates with the level of corrosive effects in that environment and the standards define or characterise environments in terms of their overall corrosion potential.

G1 Mild <300Å
An environment sufficiently well-controlled such that corrosion is not a factor in determining equipment reliability.

G2 Moderate <1000 Å
An environment in which the effects of corrosion are measurable and corrosion may be a factor in determining equipment reliability.

G3 Harsh <2000 Å
An environment is which there is a high probability that corrosive attack will occur. These harsh levels should prompt further evaluation resulting in environmental controls or specially design and packaged equipment.

GX Severe >2000 Å
An environment in which only specially designed and packaged equipment would be expected to survive. Specifications for equipment in this class are a matter of negotiation between user and supplier.

Schneider Electric Egypt and North East Africa