Search FAQs
How do I setup Anti-Jam function on the Altivar 6xx Process Drive?
Issue:
Setup Anti-Jam function on the Altivar 6xx Process Drive.
Product Line:
Altivar 6xx
Environment:
All serial numbers for Altivar 6xx
Cause:
N/A
Resolution:
To access Anti-Jam function
[Complete settings] [Pump monitoring] [Anti-jam]
[Anti-Jam Ext Trig] JEtC - Logic Input Selection
[Anti-Jam Auto Trig] JAtC - Automatic Trigger mode.
Allows you to automatically trigger the Anti-Jam on each start command, or be triggered by a time [Anti-Jam Trigger Time] JtCt or torque [Anti-jam Torque] JtCL threshold or setting.
[Anti-Jam Start Delay] JtCd - A time delay on the Anti-Jam Torque setting.
[Anti-Jam Fwd Acc] JACC - Forward Acceleration
[Anti-Jam Fwd Dec] JdEC - Forward Deceleration
[Anti-Jam Rv Acc] JACr - Reverse Acceleration
[Anti-Jam Rv Dec] JdEr - Reverse Deceleration
[Anti-Jam Fwd Speed] JFdS - Forward Speed
[Anti-Jam Rv Speed] JrUS - Reverse Speed
[Anti-Jam Fwd Time] JFdt - Time it will run in forward direction
[Anti-Jam Rv Time] JrUt - Time it will run in reverse direction
[Anti-Jam Stop Time] JZSt - Stop time between forward and reverse
[Anti-Jam Cycle Nb] JnbC - Number of cycles
[Anti-Jam Max Seq] JAMn - Limit the number of sequences
[Anti-Jam Interval] JAMt - Anti-jam minimum time between 2 non-consecutive sequences.
[Anti-Jam Error Resp] JAMb - Its response to an error/fault. Default is set to Freewheel Stop
Reference attachment for additional programming assistance
Setup Anti-Jam function on the Altivar 6xx Process Drive.
Product Line:
Altivar 6xx
Environment:
All serial numbers for Altivar 6xx
Cause:
N/A
Resolution:
To access Anti-Jam function
[Complete settings] [Pump monitoring] [Anti-jam]
[Anti-Jam Ext Trig] JEtC - Logic Input Selection
[Anti-Jam Auto Trig] JAtC - Automatic Trigger mode.
Allows you to automatically trigger the Anti-Jam on each start command, or be triggered by a time [Anti-Jam Trigger Time] JtCt or torque [Anti-jam Torque] JtCL threshold or setting.
[Anti-Jam Start Delay] JtCd - A time delay on the Anti-Jam Torque setting.
[Anti-Jam Fwd Acc] JACC - Forward Acceleration
[Anti-Jam Fwd Dec] JdEC - Forward Deceleration
[Anti-Jam Rv Acc] JACr - Reverse Acceleration
[Anti-Jam Rv Dec] JdEr - Reverse Deceleration
[Anti-Jam Fwd Speed] JFdS - Forward Speed
[Anti-Jam Rv Speed] JrUS - Reverse Speed
[Anti-Jam Fwd Time] JFdt - Time it will run in forward direction
[Anti-Jam Rv Time] JrUt - Time it will run in reverse direction
[Anti-Jam Stop Time] JZSt - Stop time between forward and reverse
[Anti-Jam Cycle Nb] JnbC - Number of cycles
[Anti-Jam Max Seq] JAMn - Limit the number of sequences
[Anti-Jam Interval] JAMt - Anti-jam minimum time between 2 non-consecutive sequences.
[Anti-Jam Error Resp] JAMb - Its response to an error/fault. Default is set to Freewheel Stop
Reference attachment for additional programming assistance
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: