This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The NBACS125 Rack Access Control appliance supports the following Proximity Cards
The NBACS1356 Rack Access Control appliance supports the following Proximity Cards
http://www.apc.com/salestools/MKEY-ADCS74/MKEY-ADCS74_R1_EN.pdf
Note: Pod Sharing with the NBACS125 / NBACS1356 Rack Access Control systems is NOT supported at this time
- H10301 - Standard 26 Bit
- H10302 - 37 Bit without facility code
- H10304 - 37 Bit with facility code
- CORP1000
NBACS125 ships with 2 x Standard 26 Bit cards. Additional packs of 10 cards (AP9370-10) can by purchased from APC by Schneider Electric.
The NBACS1356 Rack Access Control appliance supports the following Proximity Cards
- MIFAREC4 - Mifare Classic 4 byte
- MIFAREC7 - Mifare Classic 7 byte
- MIFAREDF - Mifare DESfire
- MIFAREPL - Mifare Plus
- iClass - ICLASS 8 byte
NBACS1356 does not ship with any Proximity Cards. Schneider Electric does not sell these cards at this time.
http://www.apc.com/salestools/MKEY-ADCS74/MKEY-ADCS74_R1_EN.pdf
Note: Pod Sharing with the NBACS125 / NBACS1356 Rack Access Control systems is NOT supported at this time