{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum available current on ATV12 Drive 24Vdc Power Supply?
Issue:
Maximum available current on ATV12 Drive 24Vdc Power Supply

Product Line:
ATV12, Altivar 12

Environment:
All

Cause:
N/A

Resolution:
Maximum customer current available is 100 mA (+ 24 VDC -15% +20% protected against short-circuits and overloads).

Schneider Electric Egypt and North East Africa