{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why is the refresh tags section of ENM 8.3.1 not populating the tags or the alarms are not coming in?
Issue
Alarms are not coming into ENM or the Refresh Tags will not show the PME OPC server in the refresh tags

Product Line
Event Notification Module 8.3.1

Environment
Power Monitoring Expert 8.1 or Power Scada Expert 8.1

Cause
There was an issue with the new alarm proxy interfacing properly with the Event Notification Module

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).


The ENM Patch below will upgrade ENM 8.3.1 to 8.3.2, which will resolve the issue. This patch only applies to ENM 8.3.1 and PME 8.1.

Schneider Electric Egypt and North East Africa

Attachment(s)
PME8.1_Hotfix_ENM 8.3.2.zip [17.17 KB]