Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the difference in the protection functions supported by Micro logic 1.3 M and Micro logic 2.3 M trip units used with NSX MCCB ?
The main differences between the two trip units Micrologic 1.3 M and Micrologic 2.3 M that are used with NSX MCCB are:
1- the Micrologic 1.3 M include Instantenuous Short circuit protection Function only
2- The Micrologic 2.3 M include L: Long time (thermal protection) + So: Short time with fixed time delay (Short Circuit)
Both trip units can be used with NSX 400/630 for motor application
1- the Micrologic 1.3 M include Instantenuous Short circuit protection Function only
2- The Micrologic 2.3 M include L: Long time (thermal protection) + So: Short time with fixed time delay (Short Circuit)
Both trip units can be used with NSX 400/630 for motor application
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: