{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the differences between the MA0185000 and the MA0185100 including revision?

Below are the differences between the MA0185000 and the MA0185100 including revision:

MA-0185-000

A Product introduction. No revision marking on the tap label.
B Redesign to improve return loss.
C Redesign to improve the network 75Ω impedance match. This is the lowest recommended revision that should be used.
Although it was allowed to mix the –000 revision B and C taps, performance was limited to that allowed by the older B version which did cause communication problems.
The –000 part number was obsoleted at this revision.

MA-0185-100
A No design change. Supercedes –000 Model. Logo and color change only. –100 suffix required for documentation purposes.
B No design change. Removed “F” connectors from the shipping bag.
C No design change. Internal documentation issue that standardized many product descriptions. No stock purge required.

Schneider Electric Egypt and North East Africa