Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How to I read and write the M580 SD card ?


There are  several function blocks common to both M340 and M580 which allow you to read,write and store process values.
There is sample documentation showing how these function blocks would be deployed. There is also an LD section attached with a Word document showing the logic.
The LD section was created using Control Expert (formerly Unity Pro)


R-122018




Schneider Electric Egypt and North East Africa

Attachment(s)
Read_Write_SD.pdf [615.2 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: