Issue:
SoMove, ATV61 to ATV630 conversion
Product Line:
Altivar 61 to Altivar 630
Cause:
Customer wanted to know if ATV61 files/programs can be converted to ATV630 series drive
Resolution:
Unfortunately SoMove is not able to convert files for the obsolete ATV61 drive into the ATV630 drives. The conversion will have to be done manually.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for:Schneider Electric Egypt and North East Africa