{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: What is the difference between Model 6 Standard and Industrial MCC's?
Both the Standard and Industrial MCC can be ordered in enclosure types NE MA 1, 1 A, 12 or 3 R. The Standard package lets you tailor the MCC by selecting only the options needed for an individual project, providing optimal cost / value balance. The Industrial package includes options most commonly requested and specified for industrial customers. Offering the options as part of a package reduces the possibility of leaving out common industrial features. This list represents the comparison of the two packages.
Structure FeatureStandard PackageIndustrial Package
Vertical Ground Bus MaterialSteelCopper
Horizontal Bus MaterialTin-plated Aluminum (1)Tin-plated Copper
Premium Barrier System (2)OptionalOptional
Unit FeatureStandard PackageIndustrial Package
Unit Fish tape Plugs (3)OptionalIncluded
Interior ColorGrayWhite
NameplatesOptionalIncluded
X 1 and X 2 wired to terminal blocksOptionalIncluded
(1) Exceptions: 1600-3200 Amp are Tin-plated Copper
(2) Structure Premium Barrier System; formerly Fish tape Barriers
(3) Unit Fish tape Plugs are not required when Premium Barrier System is provided

Schneider Electric Egypt and North East Africa