{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the PM8000 Series Home Screen be Modified
Issue
User would like to change the parameter on the Summary Screen or choose a different screen when the home button is pressed.

Product Line
PM8000 Series

Environment
Front Panel

Cause
The system screens are hard coded in the firmware

Resolution
There is no way to change the default summary page. The Volts mode parameter determines the voltage parameter displayed on the summary screen. If the Volts mode is set to Delta it will display Voltage Line-to-Line (Vll). If the Volts Mode is set to Wye it will display Voltage Line-to-Neutral (Vln). A user can create custom screens to display desired information, however this will always be under the custom display menu on the front panel. For instructions on how to create a custom screen, see PM8000 series meter custom screens .

Schneider Electric Egypt and North East Africa