{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Sepam 20 - why is "CCA630" displayed even though I have connected a CCA634 CT adaptor?
For the Sepam 20 range, as of firmware version V11.14 and SFT2841 software version V15.1, the Diagnostics screen will always show that a CCA630 is present.

The display will not show that a CCA634 is present, even if you have connected it correctly.

This is not a problem, and you can use the CCA634 as stated in the User Manual, provided that your Sepam 20 was manufactured after June 2006.

AEDL3

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.