{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Sepam 80 - pulse mode for Logic Outputs. What is the default pulse width for this mode?
For the Sepam 80 (and Sepam 60) relays, the pulse width for certain Logic Outputs can be set in SFT2841.

By default, the pulse width for the O1 tripping output is 200 milliseconds.  For certain other outputs on the MES120 input / output modules such as O101, this default width is 300ms.

Please see the attached file for details.  The results in the attached file were tested using firmware version V8.xx and SFT2841 software version V15.1.

AEDL3

Schneider Electric Egypt and North East Africa

Attachment(s)
Sepam80_Pulse_Mode_Logic_Outputs_BFO-Case-31146496.docx [191.71 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.